menu

Leviton Home Solutions

Basement

Recommended Basement Products

Previous
Next

Sensors

Leviton offers a wide selection of sensors, including humidity sensors, as well as occupancy and vacancy sensors, commonly referred to as "motion sensors. These state-of-the-art devices use passive infrared, ultrasonic or a combined multi-sensing technology to enhance convenience, security and provide smart energy saving solutions.

Humidity Sensor and Fan Control

Environmental safety can be a concern in bathrooms and basements. Our Humidity Sensor and Fan Control continuously monitors the air in the room and automatically turns on the ventilation fan when it detects a rise in humidity. This helps lessen the occurrence of mold/mildew for a more comfortable environment.

Vacancy Sensor

Vacancy Sensors require the user to manually turn the lights ON when entering a room; the lights will automatically turn OFF when the space is vacated, helping to save energy. The device controls Incandescent, LED, CFL and Halogen bulbs as well as motor loads.

LED Ceiling Motion Sensor Lampholder

Our LED Ceiling Motion Sensor Lampholder is the energy-efficient way to ensure that lights are on only when the space is occupied. It automatically switches lights on when motion is detected and off after 3 minutes of inactivity allowing for hands-free convenience. It’s a smart solution for saving energy and money.

Switches

Switches turn lights, fans, and other motor loads on and off. Switches come in several forms including toggle style and rockers styles.

Decora® Rocker Switch

Legendary for their streamlined elegance and smooth operation, Decora Rocker Switches have a look and feel to enhance any décor at a very modest cost. Designed from quality materials, they ensure years of trouble-free service.

Renu® Switch

The Renu® switch is part of Leviton’s colorful collection of devices featuring faceplates that easily snap on and off for instant color changes without the need to rewire. Renu® switches come in 20 popular designer colors with a matt finish, making them the easy way to add personal style to any room.

Outlets

Outlets are used as a source of power for electrical loads that are plugged into them. There are different models to address different needs. There are outlets to help provide a safer living environment, help protect against electrical shock and fire, power up today’s mobile devices, illuminate in the dark, withstand the elements outdoors and protect sensitive equipment from power surges.

AFCI Outlet

AFCI Outlets help provide protection from electrical fires by recognizing potentially hazardous arc-faults that can occur anywhere in the home’s electrical system. If a potentially dangerous arc-fault is detected the device will trip, alerting homeowners so they can investigate further.

Self-Test GFCI Tamper-Resistant Receptacle

GFCI Outlets help protect people from electrical shock due to ground faults and are required in all wet or damp locations of the home. The SmartlockPro® Self-Test GFCI adds an extra level of safety by performing a periodic self-test to confirm protected power is available.

Decora® Tamper-Resistant Outlet

Tamper-Resistant (TR) Outlets help protect children from electrical hazards that can occur if they attempt to insert a foreign object into an outlet and are an important upgrade when replacing standard outlets. Decora® outlets have a contemporary appearance and are quick to install.

Renu® Outlet

The Renu® outlet is part of Leviton’s colorful collection of devices featuring faceplates that easily snap on and off for instant color changes without the need to rewire. Renu® outlets come in 20 popular designer colors with a matt finish, making them the easy way to add personal style to any room.

Surge Protective Outlets

Surge protective products help protect your sensitive electronic equipment against both external and internal generated power surges. Surge protective outlets are typically used with computers, smart appliances and other sensitive electronic equipment located within a home office.

Surge Protective Power Strips

Surge protective power strips help protect your sensitive electronic equipment against both external and internal generated power surges. Surge protective power strips are typically used with computers, smart appliances and other sensitive electronic equipment located within a home office.

Dimmers

Dimmers help to create the perfect ambiance within a room and are available in a wide variety of designs. Dimmers help conserve energy and to reduce overall energy costs by controlling the latest in advanced bulb technology.

Decora® 1000W Digital Dimmer w/ Bluetooth® Technology

The Decora® Digital Dimmer with Bluetooth® Technology takes traditional lighting control to the next level by combining a dimmer and a timer into one smart device and allowing you to wirelessly control lighting within a 30-foot* range without the need of a hub, gateway or internet connection.

SureSlide® Universal Dimmer

Decora® SureSlide® universal dimmers provide smooth, slide-action, full-range dimming for incandescent and dimmable LED and CFL bulbs. Featuring slide-to-off functionality, this dimmer is designed for users who choose to adjust lighting levels each time the device is used.

IllumaTech® Universal Dimmer

IllumaTech® universal dimmers feature a low-profile fluid slide bar movement for fine adjustment of light levels that’s accompanied by an easy-to-use ON/OFF preset switch. The device is equipped with a dedicated switch to control a wide range of dimmable LED, CFL, and Incandescent bulbs.

Decora® Rocker Slide Universal Dimmer

With its contemporary design, this dimmer combines a Decora® rocker switch with a full-range slender slide bar for precise lighting control. The Decora® Rocker Slide Dimmer provides smooth slide-action, full-range dimming for Incandescent, and dimmable LEDs and CFL bulbs.

Surge Protection

Surge protective products help protect your sensitive electronic equipment against both external and internal generated power surges.

Surge Protective Panel

Surge protective products help protect your sensitive electronic equipment against both external and internal generated power surges. Surge protective panels installed in your basement is the second line of defense against power surges when using a tiered surge protection approach

Surge Protective Power Strips

Surge protective power strips help protect your sensitive electronic equipment against both external and internal generated power surges. Surge protective power strips are typically used with computers, smart appliances and other sensitive electronic equipment located within a home office.

Surge Protective Outlets

Surge protective products help protect your sensitive electronic equipment against both external and internal generated power surges. Surge protective outlets are typically used with computers, smart appliances and other sensitive electronic equipment located within a home office.

Do you have a question or comment?
Your message has been sent. We will contact you shortly with a reply.

From the Blog

Get Inspired